Create custom multistreams using profiles for Samsung cameras

The parameters of secondary streams (multistreams) that can be created in exacqVision are defined by the stream profiles defined in Samsung cameras. Samsung cameras ship with default profiles like H.264, MJPEG or mobile. These profiles each define a codec, default resolution and default framerate.

For example the default camera profiles may not provide a second H.264 stream. If two H.264 streams are required, the administrator can go to the camera’s configuration web page and modify or add an additional profile with the desired attributes. Once created in the camera, this profile will be available for selection in the exacqVision camera configuration page when creating a multistream.

<br>