Auto Export to a Network Share from Linux-based Exacq Server

To configure auto export from a Linux-based Exacq Server to a network share, complete the following steps: (Windows procedure here)<br><br>

NOTE: For Linux-based systems, this procedure is available in exacqVision Server/Client version 6.6 and later.<br><br>

  1. On the Archiving page in exacqVision Client, add a new archiving target with appropriate credentials and verify that it successfully connects. Do NOT configure an archiving task for this target.
  2. On the Auto Export page in exacqVision Client, click the Refresh Status button once to ensure that the configured target will be presented as an available auto export location.
  3. When you configure an Auto Export profile (or click the Auto Export Now! button), your network target will be available in the Export Path or Partition drop-down list.<br><br>

To remove the network target, complete the following steps:

  1. On the Archiving page in exacqVision Client, delete the archive target.
  2. On the Auto Export page in exacqVision Client, click the Refresh Status button once. The target will no longer be available as an Auto Export location.

<br>