Features gained by upgrading from HDVR to exacqVision:
- 2-way audio added for certain cameras (see camera database to determine which cameras support this feature).
- Remote server update is now accessible.
- Archiving features available on Windows 7 systems (not supported in Windows XP).
The Exacq 6.0 Bundle installer consists of three components:
- Server
- Client
- Web Service
This HDVR replacement bundle installer requires user intervention to complete the process. This document includes procedures for each component’s installer. After the HDVR installers are replaced with the exacqVision installers, use exacqVision versions for all future installations.
NOTE: After the migration, you will see the exacqvision “V” logo instead of the HDVR logo in all icons and shortcuts.

exacqVision Server
If the installer detects a previous HDVR server installation, a licensing message appears.

Click OK to install exacqVision Server over the existing HDVR server installation. This will install to C:\Program Files\HDVR, and video will be saved to existing directories.
exacqVision Client
If the installer detects a previous HDVR client installation, a warning message appears:

Click OK to install exacqVision Client over the existing HDVR client installation. This will install to C:\Program Files\HDVR, and all configuration XML files will be saved and applied to exacqVision Client.
exacqVision Web Service
If the installer detects a previous HDVR web service installation, a warning message appears:

Click ‘Yes’ to uninstall LightTPD and install Apache for better performance. You will lose configuration settings. See https://exacq.com/support/specsheets.php?perma=exacqVision+User+Manuals for configuration instructions.
<br>