How to update the M-Series recorder

** IMPORTANT **
Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information.

M-Series recorders currently can be updated using two methods.

  1. If the M-Series unit is connected to the Internet, simply use the client software (either local or remote)
    • Click the Configuration button (gears)
    • Click Configure System
    • Click the Update tab
  2. If the M-Series is not connected to the Internet, you can download the ARM version of the exacqVision server from https://www.exacq.com/reseller/legacy/?file=Legacy/
    • Once downloaded, put the files on a USB drive
    • Open ‘LX Terminal’, which can be found in the top menu of the operating system on the left side
    • Run the following commands to become admin
      • su admin
    • Enter the admin password (admin256 – default)
    • Navigate to the mountpoint of the thumb drive
      • cd /media/usb/
    • Execute the command to upgrade
      • sudo dpkg -i nameoffile (usually exacqVisionServer-xxx.deb, where xxx is the version number)

** IMPORTANT **
Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information.

<br>

Related Articles

<br>