ESM API api/docs does not support file upload/download

Description

If using esm api docs at /docs/api, any file upload/download action will not work.

The documentation does not even provide the correct input to upload/download files.

<br>

Version Introduced

v3.8.0.89234

<br>

Platform

All.

<br>

Steps to reproduce

  • Navigate to http://esmhost/docs/api, once fully loaded,
  • Click on system
  • Click on [GET] /api/system/logs/bundle/
  • Click on [Try it out!]

<br>

Expected result

  • File is downloaded during file download
  • Upload button/handle is provided to upload file

<br>

Actual result

  • Documentation page will just try to display the contents of the file on download.
  • There is no upload button/handler

<br>

Work around

  • Get logs using browser at http://esmhost/api/system/logs/bundle, OR use command line tools to get logs from http://esmhost/api/system/logs/bundle
  • This is the same for any other file upload or download

<br>

Version fixed

19.09.0

<br>

ESM-API-api-docs-does-not-support-file-upload-download.pdf