Does the exacqVision Server support automatic burning of video files to CD/DVD or USB?

Yes, exacqVision’s Auto Export profiles allow you to automatically burn a specified video event to a writable CD, DVD, or USB thumb drive. This function can easily be associated with a soft trigger button in the exacqVision Desktop Client using Event Linking.

CD/DVD writing is a one-time operation for each export. If using a USB thumb drive, Auto Export may be performed multiple times up to the drive capacity.

Auto Export is performed on the server, so the media you choose must be inserted into the NVR, not your Client workstation.

View our User Training Videos on Auto Export and Event Linking, or refer to the exacqVision User Manual for more information

<br>