Can I install Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder I’ve already purchased?

No, Kantech EntraPass cannot be installed on recorders that were purchased prior to February 9, 2016 without the CSA option.

If a server was previously ordered with the CSA upgrade, you can obtain the installation and registration code from Kantech technical support or from the Kantech website registration.

You may also view the FAQ page on the ExacqVision Kantech-Onboard Integration page for more information.

<br>