NOTE: This article is a reference for Legacy Exacq Mobile 3 users. Users capable of upgrading their exacqVision Server to version 24.09 and higher should refer to the article: Accessing exacqVision from Tablets and Phones using the exacqVision Mobile App on using the exacqVision Mobile app.
Exacq Mobile 3 receives live and recorded video from the exacqVision Web Service that is connected to the exacqVision recording application.

<br>
The Exacq Mobile 3 app allows you to use Apple or Android tablets and smartphones to view live video from an exacqVision server, search for recorded video, and more. To access your exacqVision server over the internet from Exacq Mobile 3, additional configuration is required. The exacqVision Web Service must be installed and configured, and the web server must be accessible through the internet.
<br>
The following steps provide an overview of the process required to deploy Exacq Mobile 3 in your environment:
- The web service can be installed on the Exacq NVR server or on a separate server. See the exacqVision Web Service User Manual for more details on installation and configuration.
- By default, the exacqVision Web Service listens on port 80. This can be modified as needed.
NOTE: A static IP address or DNS name resolution for the web server is recommended to ensure clients can consistently connect from the Internet. - Install and configure the Exacq Mobile 3 application on your device. Compatible devices and configuration steps are described in the Exacq Mobile 3 User Manual.
<br>
If you have completed these steps but you cannot see video from Exacq Mobile 3, perform the following troubleshooting steps until the issue is resolved:
- On the web server, open a browser and go to the address 127.0.0.1. (If you have changed the port from the default of 80, add a colon and the port number, such as 127.0.0.1:81.) If the exacqVision Web & Mobile Solutions login page does not load, the exacqVision Web Service is not running or is not properly configured on the server.
- If the page does load, open the web browser on your mobile device using the cellular data connection instead of WiFi. Load the externally accessible web address of the web server. If the exacqVision Web & Mobile Solutions login page does not load, the name resolution or internet connectivity of the web server is not properly configured on the server.
- If the page does load, open the Exacq Mobile 3 app and confirm the address and port settings for your server.
- If these steps to not resolve the problem, contact Exacq Technical Support.
<br>
See also:
Exacq Software/Service Connections Diagram
Example Network Diagram for Dual NIC Systems
<br>