Exacq Mobile 3 Microphone Support

Microphone support, for sending audio from your device to an exacqVision Server, was added in Exacq Mobile 3, version 8.4.

All installations of Exacq Mobile 3 acquired from Google Play and the Apple App Store support sending audio to an exacqVision Server.

<br>

Important Note

To send audio to an exacqVision Server using the mobile site, accessed via a web browser, the device or computer that is being used must have a microphone connected, the service must be hosted using HTTPS, and the site must be accessed via HTTPS. If you are accessing the mobile site over HTTP the option to send audio is not available due to browser security constraints.

<br>