Description
The HBA (Host Bus Adapter) can get damaged by the HBA clamp. Specifically the SATA 3 port capacitor can get damaged.
<br>
Note: The damage to the HBA does not affect all units. This has been seen in a very limited number. The clamp is there for shipping purposes only can may be removed. The card can become damaged only during shipping.
<br>
Platform
A-Series systems with more than 4 drives (non raid)
Note: A-Series IP only systems do not use a hold down bracket for the HBA after 11/01/2016.
Note: A-Series Hybrid systems use a modified hold down bracket for the HBA after 11/01/2016.

How to determine if the HBA is bad
- The 4 drives connected to the HBA will be labeled with /dev/sdx. The motherboard drives will have /dev/csmi in the path.
- Note: If the drives labeled /dev/csmi (motherboard drives) show offline on the Storage ==> Hardware tab, see KB https://exacq.com/kb/#loadAnswer~d8c08cb4-94a7-431c-1e9c-57f3bb7b7600
- The broken capacitor on the HBA may only affect SATA port 3 on the HBA. This ‘should’ be the 2nd drive (numbered 0-3)(drive E: or SDC ). So only one of the first 4 drives which should be drive 2 will show not found or drive errors.
- In some cases all 4 drives will show offline
- Windows servers typically will not boot at all. Linux servers will boot but will either have drive missing or drive I/O errors.
If you suspect a bad HBA
Windows
- Un-clamp and pull the HBA card leaving drives attached
- Try to boot the computer
- If it boots, then the HBA is bad
Note: they should leave the HBA clamp off whether we replace the HBA or not unless it is an hybrid system with the modified HBA clamp.
<br>
Linux
- Open up the system
- Examine the HBA card for a broken SATA 3 capacitor and/or swap SATA 3 with another port to see if it comes online after powering up.


<br>
Drive-not-found-HBA-issue.pdf