Arecont Video Shows Artifacts, Change Key Frame Interval

Symptom:

Video from an Arecont camera may display ghostly artifacts.

<br>

Problem:

Some Arecont cameras have the key frame interval, sometimes referred to as GOP, set to a high value. 

If there is a not a setting available for this in the camera’s web interface the only way to change this is through the use of CGI commands. 

<br>

Solution:

Open a web browser on the server.

Using the URL address field in the browser, enter each of the following commands replacing CAMERA_IP with the address of the camera. 

http://CAMERA_IP/set?keyframe=”on” 

http://CAMERA_IP/get?keyframeinterval 

http://CAMERA_IP/set?keyframeinterval=(1-100) 


For example, to change the interval to 10, enter: http://CAMERA_IP/set?keyframeinterval=10

Note: The lower the key frame interval, the more bandwidth will be required for the camera stream.

<br>

Arecont-Video-Shows-Artifacts-Change-Key-Frame-Interval-2.pdf