Description At times is may be necessary to change the exacqVision Web Server Logging Level. By far the most common usage is changing from the default Error logging level to Debug and then back again. Product exacqVision Web Server Solution In order to assist with troubleshooting exacqVision Web Server issues it is sometimes… Continue reading Changing the Logging Level for exacqVision Web Server
Tag: Web Service Configuration
Limited Features available in the Thin Client .
This is not an exhausted list.Soft Triggers are not available in the Web Browser/Thin Client. Customers should use the Exacq Mobile 3 Client from a Web Browser instead. The physical triggers are located in the menu of the mobile browser instead of on the live view. For Example: If you are using a trigger for… Continue reading Limited Features available in the Thin Client .
ExacqVision Web Server Relay Service Issue
Description How to diagnose if the Fast Reverse Proxy Client (FRPC) is the source of issues with the ExacqVision Web Server relay service. Product ExacqVision Web Server Troubleshooting FRPC FRPC provides a proxy service for Relay Connections used by ExacqVision Web Server. This eliminates the need for firewall configuration and prevents exposing the NVR directly… Continue reading ExacqVision Web Server Relay Service Issue
Manually Enabling Remote Web Service Configuration
THIS ARTICLE HAS BEEN DEPRECATED By default, exacqVision Web Service restricts configuration to the browser on the local machine. Through the configuration, a user can disable this restriction to enable remote configuration. However, there could be a need to manually remove this restriction (such as when installing the Web Service in a virtual environment, such… Continue reading Manually Enabling Remote Web Service Configuration
How to change web service ports
There are two ways to modify the ports used by the Web Service: It is recommended to use the configuration interface, whenever possible. However, it is possible that you must hand edit the configuration in cases where the Web Service cannot start (for example, if there is a port conflict). This article provides instructions for… Continue reading How to change web service ports
Using the ExacqVision Web Service to Connect to a Server on a Non-default Port
<br>