Factory default E-Series encoders not discoverable on Una LC-Series server

Affected platforms Una LC-Series with exacqVision 7.2 <br> Symptom Factory default E-Series encoders are discoverable through UPnP on the same subnet, but do not respond to WS-Discovery requests across subnets unless a DHCP server is present. On an Una POE port a DHCP server does not exist, so discovery only works on the same subnet,… Continue reading Factory default E-Series encoders not discoverable on Una LC-Series server