System watchdogs while archiving when SMB network share connection is lost

Affected platforms exacqVision 7.1.23 to 7.2.0 running on Ubuntu Linux <br> Symptom If the recorder is archiving and cannot reach an SMB archive target, the recorder will become unresponsive and watchdog reset. <br> Workaround Downgrade to a version prior to 7.1.23 <br> Resolution Upgrade server to 7.2.1 or newer to address proper timeout detection and… Continue reading System watchdogs while archiving when SMB network share connection is lost