Adding SCP to Illustra Essentials C2C Cameras

Description  Illustra Essential cameras were manufactured by Topview and do not include scp (Secure Copy Protocol).  As a result, files cannot be easily transferred to or from the device.  The debug.sh script can be used to temporarily install scp onto the device enabling up/downloading of files.  While scp will not survive a reboot the debug… Continue reading Adding SCP to Illustra Essentials C2C Cameras

Moving Files From Cloudvue Gateway to Windows

Description  At times it may be necessary to move or copy files from a Cloudvue Gateway to a local machine. WinSCP Portable establishes an SSH  connection between a machine running Windows and a Gateway.  It offers a convenient side by side file explorer view of the local and Gateway directories and files making it simple to… Continue reading Moving Files From Cloudvue Gateway to Windows