Exacq server is sending a DHCP discovery message on the network with different Mac address.

Description  Exacq server installed on Windows is sending a DHCP discovery message on the network using different Mac address. Exacq logs Wireshark logs Product  ExacqVision server “All versions” Solution Set a Windows Firewall outbound rule to block the DHCP port 67 on UDP. assign the IP manually to Exacq server NICs.

TDVR8016E Output stops showing Video

Description Server connected to a monitor via output form the Capture Card stops showing video on the monitor when updating to 23.09. Product Exacq Server 23.09 Steps to Reproduce Output works on Server 23.06Update to 23.09 and the Capture Card output stops showing any video on any spot monitors. Expected Results This should work. Actual… Continue reading TDVR8016E Output stops showing Video

macOS Client Live Views are 1/16th to 1/4 of the Normal Size

Description When running 23.03 Exacq Client on Mac some cameras intermittently show up very small in live view. Instead of filling the available space, they are 1/16th to 1/4 of the view area and the rest is black. Macs running two different versions of macOS (Sonoma and Big Sur) have been seen. Product Exacq Client… Continue reading macOS Client Live Views are 1/16th to 1/4 of the Normal Size

Windows Firewall Rules to prevent Failover / Failback function issues

By default VFBA uses port 28774 and TCP to communicate with EM and the Server from the Spare NVR. Rules need to be configured for outbound and inbound firewall rules on the SPARE server for failback to work as expected. To check the settings Open up Windows  Defender Firewall with Advanced Security and click on… Continue reading Windows Firewall Rules to prevent Failover / Failback function issues

EM server can’t update the web service and showing “Remote Restriction”

Description When connecting the web service to the EM server, The EM server can connect to the web service. However, it can’t push an update to it or remotely administrate the web service and keeps going back and force between “Remote Restriction” and “Running” Solution This issue has been fixed on Enterprise Manager Version 23.03.103… Continue reading EM server can’t update the web service and showing “Remote Restriction”