Replacing a Drive in Ubuntu 20.04 or later, Using GParted (Legacy)

This procedure is applicable to replacing the primary hard drive of a Linux-based exacqVision system. It assumes that the operating device is installed to an on-board flash device. Do NOT use this procedure when simply adding a drive to a system.

Using gdisk to Fix Backup GPT Table Errors in Linux  

Description  When experiencing Errors partitioning additional storage after a RAID array has been expanded or partition issues with either Archiving or Extended storage drives on an S-Series Server.  Check the partitions for errors using parted.  Product  Steps to Reproduce  Expected Results  The results return the partition layout on all block devices with no Errors   Actual… Continue reading Using gdisk to Fix Backup GPT Table Errors in Linux  

ExacqVision Corrupt Backup GPT Table or GPT Header

Title ExacqVision Corrupt Backup GPT Table or GPT Header Description  Meaning of Corrupt Backup GPT Table or GPT Header message Product  ExacqVision Server Information Similar to a ‘Bad Superblock’, this metadata information about a partition can normally be restored without losing data. Solution Run ‘gdisk’ See Knowledge Base Article #7812 “Using gdisk to Fix Backup… Continue reading ExacqVision Corrupt Backup GPT Table or GPT Header