Adding SCP to Illustra Essentials C2C Cameras

Description  Illustra Essential cameras were manufactured by Topview and do not include scp (Secure Copy Protocol).  As a result, files cannot be easily transferred to or from the device.  The debug.sh script can be used to temporarily install scp onto the device enabling up/downloading of files.  While scp will not survive a reboot the debug… Continue reading Adding SCP to Illustra Essentials C2C Cameras

HTTPS for Illustra Essentials / Dahua cameras

To set the HTTPS mode for Illustra Essentials and any Dahua OEM cameras: Go to camera web pageEnable the HTTPS option in the Network/Connection section The camera will auto generate a self-signed certificate so that exacqVision may connect with HTTPS. Note that if the camera is in HTTPS mode and the camera’s IP address is changed,… Continue reading HTTPS for Illustra Essentials / Dahua cameras