Cloudvue NVR Recorder Debugging

Description  At times it can be useful to get nvr-recorder debug level output to troubleshoot recording issue on a Cloudvue Gateway.  This can be achieved using the smv-record debug engine. Product  Solution The basic steps are: Example Tech Tip:  Support Diagnostics also captures this information in the Smartvue-smv-record.log section.

How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer

C# or other managed applications created with Visual Studio 2005 or newer cause a System.AccessViolationException in the EVAPI_CreateWindow function on Windows Vista and Windows 7. To avoid this while debugging within Visual Studio and during application execution, complete the following steps. After the project has loaded, select the project properties under the Project item on… Continue reading How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer