Description: We have seen where ExacqVision is reporting a false alarm on the hardware page with systems that have the OS on RAID. The system drives show up RED in the GUI. This is a result from storcli reporting back “unkown” for the temperature. Product: The option for OS on RAID is available for all… Continue reading OS on Raid reporting false alarm.
Author: Brian Bennett
Windows 10 Hostname
Description From the June 2022 release to the March 2023 release, the Windows 10 hostname will be the default randomized/generated one by Windows, usually something like “DESKTOP-XXXXXXX” instead of the serial number, which either “ERXXXXXXXX” or “CCPXXXXXXXX”. The fix is planned for the March release of 2023. This issue affects images for the following release… Continue reading Windows 10 Hostname