Onvif mis-handle partial socket receive and could cause delay in connection

Description

This bug caused the Onvif configuration failed to handle a complete soap message when they are partially send. The end result is that there would be a long delay before the camera would be “connected”

<br>

Version Introduced

r34959 (dev build 5_1_9_34964)

<br>

Platform

All

<br>

Steps to reproduce

Use the Hitachi DI-CB320G(F8-48-97-9E-76-9E 10.16.11.47:8080 root/admin) for testing.

connect the camera with Onvif plugin.

<br>

Expected result

Camera connected with minimum delay.

<br>

Actual result

Camera in “connecting” state for long time(could be 10-20 minutes) and finally connected.

<br>

Work Around

none

<br>

Version Fixed

r103397 (dev build 8.1.8.103450)

<br>

Keywords

Onvif