Mobile OEM Toolkit produces invalid iOS packages when the OEM does not include support for Push Notifications

Affected platforms

Mobile OEM Toolkit v1.3.1.8525

<br>

Symptom

If an OEM is attempting to create an iOS package using the Mobile OEM Toolkit v1.3.1.85257 and does not have their iOS provisioning profile set up for Push Notifications, the OEM will be unable to submit the application to iTunes Connect.
This script error will cause the web client to stop processing, displaying no servers loaded in the server list and rendering the web client non-functioning.

<br>

Workaround

Set up Push Notification support and update the provisioning profile used to generate the OEM toolkit iOS package.

<br>

Resolution

Update to OEM Toolkit v1.3.2.86528