How to Determine if a Drive is Read-Only

In Linux systems a filesystem error may cause a storage volume to be re-mounted by the operating system as Read-Only. This could be evident on the Storage page under the Drives tab when the volume status changes to ‘Write Error’ or when you attempt to search for video and find the system does not appear to be recording recent video.

<br>

How can you determine if the volume is now Read-Only?

Make a note of the volume you suspect as being Read-Only. Open a Terminal window and change directory to that volume. If the storage label is /mnt/edvr/1, enter:

cd /mnt/edvr/1

Attempt to make a new file in this location by entering:

sudo touch test.txt

If the command prompt returns without any other message, the file was created successfully and this volume is not currently in a Read-Only state.

If you get a return message that the file was unable to be created because it is Read-Only you may want to run fsck on the volume to try to correct any filesystem errors and remount it.