Removing exacqVision Server Dependency from RTSP Server Integration (Windows Only)

Issue

This article applies only to the stand alone RTSP Server Integration not the built-in RTSP support available in exacqVision Server version 19.12 and higher. 

The original stand-alone RTSP Server has the exacqVision Server listed as one of its dependencies.  This causes scripts to fail and has been observed to prevent the following: 

  • Failover/FailbackĀ 
  • Silent InstallĀ 
  • Remote Update

<br>

Resolution

To remove exacqVision Server dependency from RTSP Server integration. (Windows Only)

<br>

Stop RTSP Server service.

  • Open services.msc.
  • Find and click on service with name “exacq RTSP Server”.
  • Click stop.

<br>

Back up the registry.

  • Open regedit.exe. Note: Administrator access may be needed
  • Right-click “HKEY_LOCAL_MACHINE” and click “Export”.
  • Save exported “.reg” file.

<br>

Update the registry entry for exacq RTSP Server.

  • Double-click the exacqRTSP.reg file
  • This will remove the integrations dependency on exacqVision Server automatically.