This tutorial video showcases the new metadata updates on the exacqVision Configuration Calculator.
Missing Cloudvue Data Centers
Description When converting an Illustra camera to Cloudvue mode no Data Center entries appear in the dropdown menu. Product Steps to Reproduce Expected Results Actual Results Solution Reason #1 If the camera firmware is the cause then try using new camera firmware or if one is not available downgrading it to an earlier version. See related… Continue reading Missing Cloudvue Data Centers
Windows 7 Remote Connections
Description Windows 7 is running into an issue with the Connectivity Status showing Pending: Testing Tunnel (2). Product Steps to Reproduce Update Server/Client to latest version on Windows. Solution Windows 7 is no longer on our list of Supported versions: exacqVision Professional Video Management System Software | Exacq from Tyco Security Products FRP is a… Continue reading Windows 7 Remote Connections
Associations Not Allowed to be saved as Momentary or Sustained Option
Description When setting up a new association there is no options in the drop down menu for Momentary or Sustained when setting up Associations. Display only is seen as the only option available. This was exhibited on Server/ Client software starting on 23.09 through 24.12.7. Product Steps to Reproduce Upon update from 23.06 Server/Client to… Continue reading Associations Not Allowed to be saved as Momentary or Sustained Option
AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
Description AVCostar formerly Arecont brand Camera Models AV20576RS using firmware 65432 on versions of exacqVision 23.03.3.0 or later fail to properly decode H265 format. Product Steps to Reproduce Connect this model camera on firmware version 65432 to ExacqVision version 23.03.3.0 or later and configure for H265. Expected Results Images appear as expected. Actual Results Some… Continue reading AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
Illustra Edge Analytics
This tutorial video showcases how to configure Illustra Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:40 exacqVision Client Configuration02:34 Search3:55 Event Linking
Hanwha Edge Analytics
This tutorial video showcases how to configure Hanwha Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:25 exacqVision Client Configuration02:10 Search3:12 Event Linking
Axis Edge Analytics
This tutorial video showcases how to configure Axis Edge Analytics with exacqVision.Chapters:00:00 Intro00:13 Camera Configuration01:22 exacqVision Client Configuration02:14 Search3:00 Event Linking